Hello All,
Anyone succeeded to run QT5.5(Webengine) on imx6 platform ?
We do have Building QT for i.MX6 but unfortunately configuration didn't work. It looks like we need to have old tool-chain gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12 to compile it,which is not available for download.Can we compile it with using latest 4.7 or 4.8 tool-chain version ?
Regards
Sanjeev Sharma
I have the same situation, are you solve your problem?
Unfortunately No. I am building now with yocto branch.
Today I compiled Qt 5.5.1 but there were some problems with the launch of EGLFS and QML applications, if it will solve all these issues write here
build options
./configure -v -opensource -confirm-license -no-pch -no-xcb -no-opengl -opengl es2 -device linux-imx6-g ++ -device-option CROSS_COMPILE=/media/data/dev/gcc-linaro-arm-linux-gnueabihf-4.8-2013.10_linux/bin/arm-linux-gnueabihf- -prefix / media / data / dev / Qt5IMX6 -sysroot /media/data/dev/FS.X11 -make libs -no-gcc-sysroot
changes in the qt-everywhere-opensource-src-5.5.1 / qtbase / mkspecs / devices / linux-imx6-g ++ / qmake.conf
added two lines with the paths to libraries driver gpu-viv-bin-mx6q-3.10.17-1.0.2
QMAKE_LIBDIR_OPENGL_ES2 + = /media/data/dev/gpu-viv-bin-mx6q-3.10.17-1.0.2/hardfp/usr/lib
QMAKE_INCDIR_OPENGL_ES2 + = /media/data/dev/gpu-viv-bin-mx6q-3.10.17-1.0.2/hardfp/usr/include
Hello,
I managed to build QT5, using FSL L3.14.38.
http://www.freescale.com/webapp/Download?colCode=L3.14.38_6UL_LINUX_DOCS
It was needed to use 64-bit Linux host (Debian 8.2 in my case) with huge amount of memory
(~6GB in my case).
$ MACHINE=imx6qsabresd source fsl-setup-release.sh –b build-fb –e fb
$ bitbake core-image-minimal
$ bitbake fsl-image-qt5
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Yuri,
I am more interested in building standalone QT for imx6 like mentioned Building QT for i.MX6
Regards
Sanjeev Sharma