AnsweredAssumed Answered

Upgrade from kernel 3.0.35 to 3.14.28

Question asked by Andrea Di Chiara on Oct 12, 2015
Latest reply on Oct 27, 2015 by Andrea Di Chiara

Hi,

I'm working on a var-som-mx6 board with a kernel version 3.0.35. Now I would try to upgrade it to a newer version, for example, using Yocto Dizzy, 3.14.28 kernel version. I find out that with the new version I'll have 4 NAND partition as follows:

 

0x00000000-0x00200000 : "spl"

0x00200000-0x00400000 : "bootloader"

0x00400000-0x00a00000 : "kernel"

0x00a00000-0x20000000 : "rootfs"

 

while before I have only 3 partitions (no spl). If I upgrade my NAND writing SPL and u-boot.img via tftp as follows:

 

tftpboot 0x10800000 SPL

nand erase 0x000000 0x200000

nand write 0x10800000 0x000000 0x200000

 

tftpboot 0x10800000 u-boot.img

nand erase 0x200000 0x200000

nand write 0x10800000 0x200000 0x200000

 

it will be ok?

thank you for the attention,

best regards

Andrea

Outcomes