Hi,
Now that I have gotten my Bootloader problem solved ( Thank you Ping ), I have made a little progress, but am having a download problem.
I developed a program on my Macintosh computer ( a variant of the Red-Blue blink Carlos detailed in video 3195, to flash Red Green).
I get the following error message:
An error has occurred. See error log for more details.
ilg/gnuarmeclipse/debug/gdbjtag/data/CProjectAttributes
The Macintosh computer System Information program shows this information about the USB Bus and J-Link:
USB Bus:
Host Controller Location: Built-in USB
Host Controller Driver: AppleUSBOHCI
PCI Device ID: 0x0aa5
PCI Revision ID: 0x00b1
PCI Vendor ID: 0x10de
Bus Number: 0x04
J-Link:
Product ID: 0x0105
Vendor ID: 0x1366
Version: 1.00
Serial Number: 000621000000
Speed: Up to 12 Mb/sec
Manufacturer: SEGGER
Location ID: 0x04100000 / 3
Current Available (mA): 500
Current Required (mA): 100
If someone can direct me on what to correct, it would be most appreciated,
Thanks,
Mark
Hi Mark,
do you use KDS3.0 or Codewarrior10.6?
if use KDS3.0, it can support Mac OS 10.10 ("Yosemite").
Kinetis Design Studio Integrated Development |Freescale
if use CW10.6 it doesn't support Mac OS.
CodeWarrior for Microcontrollers-Eclipse IDE|Freescale
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------