AnsweredAssumed Answered

Does i.MX6 MIPI-CSI I/F can support non-continuous clock LPS mode ?

Question asked by Apollo Chang on Oct 8, 2015
Latest reply on Jan 22, 2016 by igorpadykov

Hi

Does i.MX6 MIPI-CSI I/F can support non-continuous clock LPS mode ?

 

Yellow ---> MIPI_CSI_CLK

Green ---> MIPI_D0

 

non_con.jpg

Base on Debug steps for customer MIPI sensor.docx

 

3. Check every register of MIPI CSI-2 with MIPI_CSI_N_LANES ~ MIPI_CSI_DATA_IDS_2.

Tips:

  • In ov5640_mipi case (2 data lanes are used), the correct MIPI_CSI_PHY_STATE is 0x330 (and the bit 11 is jumping between 0 and 1, the value is jump between 0x330 and 0x300.

 

I think 0x330 and 0x300 is base on continuous clock LPS mode. Right ?

If non-continuous clock LPS mode , the value is 0x300 , 0x630 , Right ?

Outcomes