Hi,
I am working with code warriorv10.6 and MQX v4.0.
I am working on a project in which I am using SDCard demo and Web Hvac demo.
Both Demos are working perfectly.
Now what I need to do is., I am creating .txt file into SDCard and I want to access it using
PC. Say My PC address is 172.168.1.202 and I created Package.txt file into SDcard.
Now I want to access Package.txt by just writing url like: http:\\172.168.1.202\Package.txt (not exactly like this but want to use http:\\172.168.1.202\.......... )?
Is this possible to read/write into SDCard directly from PC using http protocol?
Please note that I do not want to use any shell commands or USB demo to access .txt file from SDCard.
Regards,
Utsavi Bharuchwala
Hi
I think you can access fie by writing your url. please check the section 5.10.3 about aliases in RTCS user guider.
regards
Daniel