AnsweredAssumed Answered

How to set the clock to 116 MHz on MPC5668G

Question asked by Hugo Bouchard on Oct 8, 2015
Latest reply on Oct 20, 2015 by Hugo Bouchard

Hello,

 

I'm trying to configure the clock to run at 116 MHz in a MPC5668G as follow:

 

/* System is clocked by IRC (00 IRC, 01 4-40MHz, 10 PLL)*/

SIU.SYSCLK.B.SYSCLKSEL = 0b00;

 

/*----- PLL -----*/

 

/* Enable the 4-40MHz oscilator (not necessary, done by reset) */

CRP.CLKSRC.B.EN40MOSC = 1;

 

/* Enable clock 128KHz for RTC */

CRP.CLKSRC.B.EN128KIRC = 1;

 

/*  Set ERFD to divide by 5 at first to avoid cpu overclocking -

** should not occur since system is not clocked from PLL

** Set PLL to use crystal reference (12MHz),

** EMFD=100 to multiply by 116,

** and EPREDIV=5 to divide by 6

** Result:    fvco = 12MHz * 116 / 6 = 200MHz (192-600MHz)

**            fout = 12MHz * 116 / (6 * 5) = 40MHz

*/

FMPLL.ESYNCR2.R=0x00000004;

FMPLL.ESYNCR1.R=0x70050064;

 

/* Wait for PLL lock (<400us) */

while(FMPLL.SYNSR.B.LOCK != 1);

 

/* ERFD now divides only by 6 so * fout = fvco / (ERFD+1)

* fout = 12MHz * 116 / (6 * 2) = 116MHz     */

FMPLL.ESYNCR2.R=0x00000001;

 

/*----- SIU - CLK -----*/

/* System is clocked by PLL (00 IRC, 01 4-40MHz, 10 PLL)*/

SIU.SYSCLK.B.SYSCLKSEL = 0b10;

 

However, it doesn't work. At first instruction executed after having switched system clock to PLL (last line of previous code), I get a trap. When I go step by step in the deassembly view with my debugger, the assembly instructions read by the debugger change which is wird. What's wird too is that I can configure the clock to run up to 84 MHz but at 85 MHz it doesn't work, I get a trap but the assembly code is not modified. In all cases, the CLKOUT signal is what I expected

 

I also tried to activate the frequency modulation with different setting without success.

 

The clock reference we are using is NX5032GA-12.000M if that helps.

 

I also tried the PLLinit code in AN4241.pdf but it doesn't work better. Also, is that me or is the function set a PLL at 128 MHz in this application notes?

 

Anyone can help please?

 

Thanks!

Hugo

Hello,

 

I'm trying to configure the clock to run at 116 MHz in a MPC5668G with MQX 4.1. I modified the function ClockInit in file __ppc_eabi_init.c as follow:

 

/* System is clocked by IRC (00 IRC, 01 4-40MHz, 10 PLL)*/

SIU.SYSCLK.B.SYSCLKSEL = 0b00;

 

/*----- PLL -----*/

 

/* Enable the 4-40MHz oscilator (not necessary, done by reset) */

CRP.CLKSRC.B.EN40MOSC = 1;

 

/* Enable clock 128KHz for RTC */

CRP.CLKSRC.B.EN128KIRC = 1;

 

/*  Set ERFD to divide by 5 at first to avoid cpu overclocking -

** should not occur since system is not clocked from PLL

** Set PLL to use crystal reference (12MHz),

** EMFD=100 to multiply by 116,

** and EPREDIV=5 to divide by 6

** Result:    fvco = 12MHz * 116 / 6 = 200MHz (192-600MHz)

**            fout = 12MHz * 116 / (6 * 5) = 40MHz

*/

FMPLL.ESYNCR2.R=0x00000004;

FMPLL.ESYNCR1.R=0x70050064;

 

/* Wait for PLL lock (<400us) */

while(FMPLL.SYNSR.B.LOCK != 1);

 

/* ERFD now divides only by 6 so * fout = fvco / (ERFD+1)

* fout = 12MHz * 116 / (6 * 2) = 116MHz     */

FMPLL.ESYNCR2.R=0x00000001;

 

/*----- SIU - CLK -----*/

/* System is clocked by PLL (00 IRC, 01 4-40MHz, 10 PLL)*/

SIU.SYSCLK.B.SYSCLKSEL = 0b10;

 

However, it doesn't work. At first instruction executed after having switched system clock to PLL (last line of previous code), I get a trap. When I go step by step in the deassembly view with my debugger, the assembly instructions read by the debugger change which is wird. What's wird too is that I can configure the clock to run up to 84 MHz but at 85 MHz it doesn't work, I get a trap but the assembly code is not modified. In all cases, the CLKOUT signal is what I expected

 

I also tried to activate the frequency modulation with different setting without success.

 

The clock reference we are using is NX5032GA-12.000M if that helps.

 

I also tried the PLLinit code in AN4241.pdf but it doesn't work better. Also, is that me or is the function set a PLL at 128 MHz in this application notes?

 

Anyone can help please?

 

Thanks!

Hugo

Outcomes