Hallo everyone,
i'd like to to reprogram the MPC5604E. So far i've downloaded the example software (Salsa Low Cost Reference Kit Aptina Camera version - demo SW + binaries). Now i'd like to analyse, edit and test the code. Unfortunately the example project is missing some folders (OS, Salsa). My question is: Is it possible to get these?
Any help would be greatly appreciated
Hi,
if you want to modify the sample application, Freescale Autosar OS is needed. This note is copied from SalsaLowCostRefKitLibAPI.pdf:
"For evaluation purposes the sample application can be modified. In this case Freescale AUTOSAR OS/MPC560xE v.3.0 RTM should be installed into application\intapp_xxx\OS directory where scc subdirectory is expected."
Notice that it is commercial software, it is not provided for free:
Freescale AUTOSAR Software Solutions|Freescale
Regards,
Lukas
Hi,
we want to use the OS only for educational purposes at the Ostfalia -
University of Applied Sciences. Is it possible to get it for educational
purposes?
Redards,
Thies
Am 09.10.2015 um 09:00 schrieb lukaszadrapa:
>
Freescale Community
<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>
<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>
>
Reprogram MPC5604E
reply from Lukas Zadrapa
<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQlPCh-2BdR0Iuh2b8GsySf-2BTzStW8Kcy62N7SZlPsQqm9PXJpFJHNa7nyleWxUK8Pkk-3D>
in /MPC5xxx/ - View the full discussion
<http://jiveon.jivesoftware.com/mpss/c/fAA/PDcDAA/t.1r4/NW1cNm_gSvCqUQ9CiEx2dg/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bRorSxS-2FfrSXtyorEQP4jO5nezm6ZWD5y-2FKZ8-2FwKcOI8rn6qX3JpWV904diHHmRMOg-3D>
>