AnsweredAssumed Answered

(FXTH87 Tire Pressure Monitor Sensor Family) Accelerometer Wake up

Question asked by Arvind Singh on Oct 7, 2015
Latest reply on Oct 12, 2015 by Tomas Vaverka

I am new to FXTH87 Family.

 

I ran demo code using codewarrier and measured temperature, pressure and accelerometer and are working fine.

 

Now i need to implement a functionality,

For example:- Vehicle is in parking, at that time device should go into low power mode.  and when it starts moving accelerometer will sense it any wake up the whole device.

 

In b/w what is the difference b/w these two API's

UINT8 TPMS_READ_ACCELERATION_X(UINT16 *u16UUMA, UINT8u8Avg, UINT8 u8FiltSelect, UINT8 u8DynamicOffset)

UINT8 TPMS_READ_DYNAMIC_ACCEL_X(UINT8 u8Filter, UINT8* u8Offset, UINT16* u16UUMA)

Outcomes