AnsweredAssumed Answered

Use of PXP for image color conversion

Question asked by sachin shewale on Oct 5, 2015
Latest reply on Oct 7, 2015 by Yuri Muhin

Hi,

 

We want to convert RGB image to RED/BLUE format. We are using PXP for this. Platform used: MCIMX6U8DVM10AC

Input Mode selected: DIRECT_RGB454

Output Mode Selected:  RGB888

Input Image format: RGB888

Output Image format: RGB888

 

Lookup Table Data: 16KB

Address = 8K

 

Lookup table values:

LUT Data format: RGB565

D15 D14 D13 D12 D11 D10 D09 D08 D07 D06 D05 D04 D03 D02 D01 D00

R      R    R      R     R   G      G     G     G    G     G    B      B      B     B     B

 

From 0 to 4096:

0xF800 <Red Colour>

 

From 4096 to 8192:

0x001F <Blue Colour>

 

Please check and let us know if understanding is correct.

Outcomes