Hi,
In my firmware (MQX 4.1.1) I have http and snmp servers running without problems but I need to change static IP address dynamically. If I have only http server running, this process works fine:
1) execute ipcfg_unbind
2) execute ipcfg_bind_staticip with new IP data
But if I have both http and snmp servers running at once, the ipcfg_unbind function is halted and both servers stop their execution. I have tried to call SNMP_stop before ipcfg_unbind but it didn't work. Any idea?
Thank you very much!
Hello David,
Could you please try using the RTCS_if_unbind() and RTCS_if_bind()
Description of the RTCS functions can be found in the RTCS Reference Manual.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------