AnsweredAssumed Answered

About EIM data bus width in i.MX6SL.

Question asked by Keita Nagashima on Sep 30, 2015
Latest reply on Nov 11, 2015 by Keita Nagashima

Dear All,

 

Hello.

First, refer to Table 4-2. Muxing Options in IMX6SLRM(Rev.2) (Page.211).

Data bus width looks 16bit.

 

Next, refer to Table 20-1. EIM multiplexing  in IMX6SLRM(Rev.2) (Page.763).

The description looks can setting 32bit width with Non Multiplexed Address/Data Mode.

 

[Q1]

Which is right description?

Is it possible to configure the 32bit width in Non Multiplexed Address/Data Mode?

(Is it typo in Table 20-1?)

 

[Q2]

In case of one use the 32bit data bus, is it possible to set the 32bit bus the Multiplexed Address/Data mode?

 

Best Regards,

Keita

Outcomes