Hello,
I am setting up a project in Processor Expert (KDS 3.0.1) for a MK26FN2M0VMI18 MCU
It is not possible to select pin ADC1_DP1 as input for ADC1.
Anyone that can help fixing this?
BR
Jesper P. Larsen
Solved! Go to Solution.
Hi Jesper,
I would recommend you to use Kinetis SDK 1.3 which is the latest release, in this version the ADC1_DP1 pin is now routed to the ADC1 function:
you should be able to select it as input pin for channel 1:
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jesper,
I would recommend you to use Kinetis SDK 1.3 which is the latest release, in this version the ADC1_DP1 pin is now routed to the ADC1 function:
you should be able to select it as input pin for channel 1:
Hope it helps!
Best Regards,
Carlos Mendoza
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------