We are Using P1013 power PC processor and we need to interface 16 bit DDR3 memory. But as per the P1013 datasheet it say it can support only 32/64 bit. Can you pleasd confirm if we can interface single 16 bit DDR3 with processor or we have to use two 16 bit DDR3.
You are correct, P1013 supports only 32-bit and 64-bit DDR bus interface. So you need two 16-bit devices to form 32-bit bus. Note that MDQ[0:31] data bits should be used in 32-bit case.
Regards,
Bulat