AnsweredAssumed Answered

Failed to fetch the package from git://git.freescale.com/imx/linux-2.6-imx.git

Question asked by xj li on Sep 29, 2015
Latest reply on Oct 1, 2015 by Yuri Muhin

I am trying to build yocto project for i.mx6 board on Ubuntu 14.04

when running the commands "repo init " and "repo sync", it always failed, so the relative packages were downloaded from the webpage according to the xml file.

And then when running the command "bitbake fsl-image-qt5", there existed an error that failed to fetch the package from git://git.freescale.com/imx/linux-2.6-imx.git.

I tried to run the command "git clone git://git.freescale.com/imx/linux-2.6-imx.git" in the shell, it always appeared that connection timed out. however, I can access this address by the webpage. I can't resolve it, so I need help. Thank you.

Outcomes