MQX 4.2 Cloning Wizard Name Size Limit?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX 4.2 Cloning Wizard Name Size Limit?

Jump to solution
486 Views
gorakk
Contributor IV

Is there a size limit for the Name of a cloned BSP?

I originally put a fairly long descriptive name for a new BSP - but when I tried to generate the project an error was shown.

For example - if I use a Name of: abcdefghijklmnopqrstuvwxyz0123456789

The following error is shown:

C:/Users/allwel/AppData/Local/Temp/ocr3A43.tmp/src/core/uproject/internal/_xml_utils.rb:21:in `initialize': No such file or directory @ rb_sysopen - ../../../mqx/examples/context_switch_callback/build/kds/context_switch_callback_abcdefghijklmnopqrstuvwxyz0123456789/context_switch_callback_abcdefghijklmnopqrstuvwxyz0123456789 int flash release jlink.launch (Errno::ENOENT)

Something shorter - abcdefghijklmnopqrstuvwxyz - will work ok.

Is there meant to be a size limit?

Regards,

Allen

Tags (2)
0 Kudos
1 Solution
367 Views
soledad
NXP Employee
NXP Employee

Hello Allen,

Only 32 characters can be used for the name.


Have a great day,
Sol
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
368 Views
soledad
NXP Employee
NXP Employee

Hello Allen,

Only 32 characters can be used for the name.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos