VDD_SNVS_IN connection recommendations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VDD_SNVS_IN connection recommendations

986 Views
ko-hey
Senior Contributor II

Hi all

I want to confirm about VDD_SNVS_IN recommendation.

According to the Table 2-6 of Hardware Development Guide, there are a recommendation as below.

When VDD_SNVS_IN is not powered by a battery, it is recommended that VDD_SNVS_IN = VDD_HIGH_IN.

This description means that if user don't use coin-cell battery, they should provide to VDD_SNVS_IN and VDD_HIGH_IN form same source.

Is it correct ?

Ko-hey

Labels (2)
Tags (2)
0 Kudos
1 Reply

455 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

this is not obligatory, but most suitable option.

Still one can use power-up sequence as defined by datasheet:

VDD_SNVS_IN supply must be turned ON before any other power supply.

It may be connected (shorted) with VDD_HIGH_IN supply.

...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos