can anybody provide the example project for s12g to wake up from the sci?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can anybody provide the example project for s12g to wake up from the sci?

383 Views
steven_zhang
Contributor V

can anybody provide the example project for s12g to wake up from the sci?

Labels (1)
0 Kudos
1 Reply

244 Views
RadekS
NXP Employee
NXP Employee

Hi Steven,

Please look at my example code GN32-SCI_wake_up_from_stop-CW51 here:

https://community.freescale.com/docs/DOC-93792

SCI edge is here used for wake-up from stop mode.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos