updating/flashing u-boot on LS1021A-IOT?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

updating/flashing u-boot on LS1021A-IOT?

675 Views
maclainl
Contributor II

Hi,

I have found several instructions on how to flash a new u-boot image it to the Quad SPI NOR flash on LS1021A-IOT.

Resources like this seem helpful.

How do I recover from a failed u-boot flash on the LS1021A?

FTF-DES-F1189.pdf

Freescale Technical Information Center

However, my question is this:  Is there an easy place to download the latest version of U-boot for LS1021A-IOT?  I just want a U-boot version that supports SATA on the board.  I don't want to rebuild it, or download a huge package, etc.  I just want to get the latest .bin for the board that will setup the SATA for booting Linux from the SSD.

Thanks,
Mac

0 Kudos
0 Replies