Hi,All:
freescale imx6 can use the Logitech K200 or K120 Keyboard and use mouse to point applications?(for linux QT5 yocto project)
Please help me,thanks.
I designed a board occurs problem for freescale imx6 cann't use the Logitech Keyboard K200 or K120 and use another mouse to point applications.
(it's ok About 30 seconds or press any keyboard key to point the application)
(中譯:freescale imx6可以使用羅技K200或K120的鍵盤然後用另一個輸入裝置滑鼠去點應用程式嗎?(for linux QT5 yocto project)
我設計一塊板子發生問題在freescale imx6 不能插入使用羅技K200或K120的鍵盤並且另一個uab port用滑鼠去點應用程式.
(大約要30秒或按任何鍵盤的鍵才能點應用程式)
)
I don't have K200 and K120. I have K400 (wireless) and working well on i.MX6 board.
hi,jimmychan:
I guess it should be a Logitech keyboard keycode problem.
thanks for u answer.