DDR3 chip on P1014

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 chip on P1014

651 Views
dominikfässler
Contributor I

How do I get a single DDR3 Chip (Alliance Memory AS4C128M16D3) running on a P1014? Are there any examples?

Labels (1)
0 Kudos
2 Replies

456 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

AS4C128M16D3 is a 16-bit  DDR3 JEDEC Standard Compliant device which is supported by the P1014. I am not sure what do you mean as "get a single DDR3 Chip (Alliance Memory AS4C128M16D3) running on a P1014”. Do you mean connections, layout example or register settings problem? Unfortunately I did not see the right example. But I believe the next application notes can be useful

AN3940, Hardware and Layout Design Considerations for DDR3 SDRAM Memory Interfaces

https://www.freescale.com/webapp/Download?colCode=AN3940

AN4039, PowerQUICC and QorIQ DDR3 SDRAM Controller Register Setting Considerations

http://cache.freescale.com/files/32bit/doc/app_note/AN4039.pdf

See also section 4 DDR controller recommendations in the AN4534, P1010 QorIQ Integrated Processor Design Checklist

https://www.freescale.com/webapp/Download?colCode=AN4534

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

456 Views
dominikfässler
Contributor I

Thank you for your reply. AN4039 helped a lot.

0 Kudos