AnsweredAssumed Answered

EEPROM area can't be pragramed by J-FLASH in KE02

Question asked by Const Yu Employee on Sep 22, 2015
Latest reply on Sep 23, 2015 by Const Yu

One customer is using KE02Z64VLC4, they are preparing for the Small PP. They applied the EEPROM(256bytes, the address is from 0x10000000 to 0x100000FF) in KE02 to store some configuration information in IAR, the code is as below, and after building, this area was filled right data in the S19, as below figure 2.

 

But now the problem is we found these area(from 0x10000000 to 0x100000FF) in the S19 can’t be flashed into MCU by J-flash normally. I checked the segger J-flash IDE, found no such area is defined in J-flash as below figure.

2.jpg1.jpg

So there a way to enable this function to make it possible to program the EEPROM area by J-Flash?

3.jpg

Outcomes