imx28 Battery Charger issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx28 Battery Charger issue

Jump to solution
635 Views
liyingchun
Contributor I

Hi expert

?I know that imx28 has a on chip battery charger and can charge the Li-ion battery. I want to know that if it can be used to charge the NI-MH battery ( nickel-metal hydride battery )?

I checked the AN4199 doc. It seems that it does not mention the related information.

Thanks very much!

Labels (1)
Tags (1)
0 Kudos
1 Solution
506 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically it is possible to configure i.MX28 charger for Ni-MH,

but please take a look at the following general considerations.

  http://leakeem.hubpages.com/hub/Which-is-better-Nickel-Metal-Hydride-NiMH-or-Lithium-Ion-Li-ion-batt...


Have a great day,
Yuri
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
507 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically it is possible to configure i.MX28 charger for Ni-MH,

but please take a look at the following general considerations.

  http://leakeem.hubpages.com/hub/Which-is-better-Nickel-Metal-Hydride-NiMH-or-Lithium-Ion-Li-ion-batt...


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos