AnsweredAssumed Answered

cannot connect to TWR-56F8400 - error occured while connecting to the interface hardware

Question asked by marcos1 on Sep 18, 2015
Latest reply on Sep 23, 2015 by Fiona Kuang

I have TWR-56F8400 that I'm operating standalone.

I'm physically connected to the board via USB.

The pre-loaded demo is running with LEDs blinking.

 

But when I simply follow the example from the quick start guide I already run into the issue that when I start debugging I cannot connect:

PE_connection.png

I'm using CodeWarrior 10.6.

The quick start guide instructions seem to refer to a previous version of CodeWarrior so the menu for setting up the project seems slightly different.

 

I played around with various debug settings but nothing seems to work.

 

How do figure out what the problem is?

Outcomes