Dear all,
We use i.MX6Quad.
We want to use eMMC(JEDEC4.51)device.
And we use eMMC Boot.
However, this eMMC does not support SPI mode.
Can we use this eMMC device?
For the method that eMMC(JEDEC4.51) is used in as 4.x,
I referred to the following URL.
https://community.freescale.com/message/435796#435796
However, We do not know whether we can use eMMC which does not support SPI mode.
If we can use this, can MFG tool write a program in this eMMC?
May I have advice?
Best Regards,
Yuuki
Hello,
Basically the SPI mode is not needed for eMMC operation with i.MX6.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------