AnsweredAssumed Answered

MFG Tool hangs for custom board

Question asked by Luke Marvin on Sep 15, 2015
Latest reply on Sep 15, 2015 by igorpadykov

Hi I'm trying to get the MFG Tool to program an SD card in my custom board. I've got the DDR and u-boot set up correctly but the output hangs.

 

I've posted the log in a gist:

https://gist.github.com/3fec0ebd75579eac57e6.git

 

It hangs after:

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

 

When I use the MFG Tool with the reference design we used the next lines in the log are:

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal
----enable clko2
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.

 

Is my board getting stuck in this hw-breakpoint? I'm just using the standard uImage that was in the MFG Tool directory.

Outcomes