AnsweredAssumed Answered

QorIQ T1040 Hardcoded RCW usage in "Single Oscillator Source" Reference Clock mode

Question asked by fdm on Sep 14, 2015
Latest reply on Sep 16, 2015 by Yiping Wang

Hi,

 

I'm planning to use the "Single Oscillator Source" Reference Clock mode in the T1040 based custom board currently in development.

Is it possible to use a "Hardcoded RCW" option in order to program the NOR and/or NAND flash with CW TAP during board bring-up if only DIFF_SYSCLK=100MHz is supplied and the DDRCLK dedicated pin is not connected at all?

 

BR,

   Denis

Outcomes