hi all !
i'm new in kinetis
i'm using MKL16Z128VFM4 to communicate witch max9860 codec
the codec has mclk,lrclk,bclk,sdin,sdout pins
and the mcu has I2S0_TXD0,I2S0_TX_FS,I2S0_TX_BCLK,I2S0_MCLK,I2S0_RXD0,I2S0_RX_BCLK,I2S0_RX_FS
could you show me how to connect these pins
thanks!
Hello tuan,
For i have not fund the reference manual , so i don't know the pin lrclk mean, you can check or you can send it to me .
About the other pins i guess as this below , you can refer to :
kl16 ----- MAX9860
I2S0_MCLK mclk
I2S0_TX_BCLK bclk
I2S0——TXD0 sdin
I2S0_RXD0 sdout
I2S0_SDA sda
i2s0_SCL scl
I recommend you read the RM check all of the meaning of pins .
Hope it helps!
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------