i.MX6DQ IPU IC combining performance.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6DQ IPU IC combining performance.

Jump to solution
598 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL IPU CSI.

Please see the slide No. 56 of attached file in A Deep Dive into Image Processing for i.MX 6 Series Applications Processors

It says the combining in the Image Conveter is upt to 40M pixels/sec with i.MX6DQ.

Next, please see chapter 37.1.2.1.5.3 in IMX6DQRM Rev.3, it says the IC perfomance is 200M pixels/sec for input and 100M pixels/sec for output.

To understand combining performance by Image Converter, which performance should I use?

Best Regards,

Satoshi Shimoda

0 Kudos
1 Solution
470 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

Image Conveter suppots many operations and RM gives max. IC perfomance.

IC combining performance is given in presentation.

Best regards

igor
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
471 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

Image Conveter suppots many operations and RM gives max. IC perfomance.

IC combining performance is given in presentation.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos