AnsweredAssumed Answered

DTS file customization ?? please....

Question asked by rufp0105 on Sep 11, 2015
Latest reply on Sep 18, 2015 by STEFANO BABIC

Hi,

I would like to add some SPI, I2C, Serial devices to IMX6 DL reference designs. When referring to DTB (Device Tree Blobs) generation from DTS file and referring to DTS file for example ecspi1 is lke as below:

 

 

pinctrl_ecspi1: ecspi1grp {

            fsl,pins = <

                MX6QDL_PAD_EIM_D17__ECSPI1_MISO        0x100b1

                MX6QDL_PAD_EIM_D18__ECSPI1_MOSI        0x100b1

                MX6QDL_PAD_EIM_D16__ECSPI1_SCLK        0x100b1

                MX6QDL_PAD_EIM_EB2__GPIO2_IO30          0x0b0b0    /* CS */

            >;

        };

 

 

What does this 0x100b1 specifies. How to arrive at that value. Why CS (Chip Select is given 0x0b0b0). How to calculate that value/arrive at some value. And also in some places it is like this:

 

pinctrl_usdhc1: usdhc1grp {

            fsl,pins = <

                MX6QDL_PAD_SD1_CMD__SD1_CMD        0x17059

                MX6QDL_PAD_SD1_CLK__SD1_CLK           0x10059

                MX6QDL_PAD_SD1_DAT0__SD1_DATA0        0x17059

                MX6QDL_PAD_SD1_DAT1__SD1_DATA1        0x17059

                MX6QDL_PAD_SD1_DAT2__SD1_DATA2        0x17059

                MX6QDL_PAD_SD1_DAT3__SD1_DATA3        0x17059

            >;

        };

 

in above snippet how 0x17059 came??? im no understatd...;;;

Outcomes