Kernel 3.14, video issues with supported cea mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel 3.14, video issues with supported cea mode

Jump to solution
676 Views
angelo_d
Senior Contributor I

Dear all,

i have seen that in 3-14 imx6 kernel,  the mode 1280x800 for hdmi (have Adafruit hdmi lcd with this mode) is no more supported. Kernel allows only cea mode 1280x720.

Setting 1280x800M60 in kernel boot params,

Kernel 3.11 was still allowing 1280x800 reso:

[system@localhost ~]$ cat /sys/class/graphics/fb2/mode

U:1280x800p-60

while 3.14 not, so i ged a stretched image in the hdmi display

[user@localhost ~]$ cat /sys/class/graphics/fb2/mode

S:1280x720p-60

If i set 1280x720M60 as kernel params, nothing changes. Every help is appreciated.

Best regards

Labels (2)
0 Kudos
1 Solution
545 Views
angelo_d
Senior Contributor I

Hi, found this solution

Re: How to add HDMI resolution to i.MX6 Yocto BSP.

Of course also wxga mode struct need to be added.

Thanks

View solution in original post

0 Kudos
2 Replies
546 Views
angelo_d
Senior Contributor I

Hi, found this solution

Re: How to add HDMI resolution to i.MX6 Yocto BSP.

Of course also wxga mode struct need to be added.

Thanks

0 Kudos
545 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi andelo dureghello,

I am very glad to hear of you have found the way to solve your problem. Welcome to create new threads in our community.

Have a nice day.

Best Regards

Dan

0 Kudos