I am using the netcomm ocn dma api to transfer using simple mode mem2mem. I am getting a Transfer Error, but no other information on the cause.
Is there any needed pamu/liodn changes that need to be taken cared off for simple mem2mem? The reference manual is extremely vague!
Thanks,
Mihai
Solved! Go to Solution.
I found the issue. Turns out I needed to use PAMU for mem2mem.
Thanks
Reference Manual states there is a number of number of possible reasons for transfer error - "non-correctable ECC errors on memory accesses, parity
errors on flash controller, address mapping errors, and so on". But, DMA controller itself does not offer more details, the only "Transfer Error" bit is available in SRn.
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------