Hi Sir,
I base on FSL YOCTO 3.14.28_1.0.1 code to run core-image-minimal-initramfs function.
But it still has some error message.
Which file I need to update ?
bitbake core-image-minimal-initramfs
Loading cache: 100% |###########################################| ETA: 00:00:00
Loaded 2524 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
ERROR: Nothing RPROVIDES 'initramfs-live-install' (but /home/abner/fsl-imx6-yacto/sources/poky/meta/recipes-core/images/core-image-minimal-initramfs.bb RDEPENDS on or otherwise requires it)
ERROR: initramfs-live-install was skipped: incompatible with host arm-poky-linux-gnueabi (not in COMPATIBLE_HOST)
NOTE: Runtime target 'initramfs-live-install' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['initramfs-live-install']
ERROR: Required build target 'core-image-minimal-initramfs' has no buildable providers.
Missing or unbuildable dependency chain was: ['core-image-minimal-initramfs', 'initramfs-live-install']
I am also facing the same kind of issue for dizzy branch. Please give some input regarding that.
Hello Chen Abner,
Would you please add some information on how you’re initializing the environment? Perhaps there is a problem with the building target (machine) configuration.
Hi Sir,
I use source setup-environment to init the environment.
please refer to following init log:
source setup-environment imx6qsabresd-qt5/
Welcome to Freescale Community BSP
The Yocto Project has extensive documentation about OE including a
reference manual which can be found at:
http://yoctoproject.org/documentation
For more information about OpenEmbedded see their website:
You can now run 'bitbake <target>'
Common targets are:
core-image-minimal
meta-toolchain
meta-toolchain-sdk
adt-installer
meta-ide-support
Your configuration files at imx6qsabresd-qt5/ have not been touched.