Where can I get imx6 source "L3.0.35_1.1.0_121218_source.tar.gz"?
The lastest is L3.0.35_4.1.0_130816_source.tar.
But I want to get the older source.
Hi da yuan,
I saw that you also create the same question on our Chinese website, and I already give you reply there. The version of L3.0.35_1.1.0_121218_source.tar.gz BSP is old and do not exist on website. So here you can choose the L3.0.35_4.1.0 BSP, the downloading link is :http://www.freescale.com/product ... ab=Design_Tools_Tab.
Hope this can help you.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for you help.
I want to do fast boot imx6 with lvds .
I follow by Linux Fast Boot on i.MX6 Sabresd Board,but my boot time is more than 3 sec.
I use source L3.0.35_4.1.0 BSP,Linux Fast Boot on i.MX6 Sabresd Board use L3.0.35_1.1.0 BSP.
Maybe there are something different with L3.0.35_1.1.0 BSP.
So I want to download L3.0.35_1.1.0 BSP to try.