Program "make" not found in PATH...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program "make" not found in PATH...

Jump to solution
4,132 Views
jacquesnapoleon
Contributor I

Hello,

 

I installed Kinetis Design Studio and download Kinetis KE02-SC.zip examples.

After importing the projects in IDE, all projects appear with problems and the error "Program "make" not found in PATH".

Could you please help...

 

Thanks and regards.

Labels (1)
0 Kudos
1 Solution
1,700 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jacques,

Does your KE02-SC example support KDS ?

In my hand ,it only support CW ,IAR and KEIL .

pastedImage_0.png

Hope it helps

Alice

View solution in original post

0 Kudos
6 Replies
1,700 Views
TICS_Fiona
NXP Employee
NXP Employee

Hi Jacques

The demo examples KE02-SC.zip are based on CodeWarrior, IAR and Keil. You may open or import the example project with any above IDE.

CodeWarrior v10.6.4 can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10

Or if you would import the project into KDS, please refer to this doc under your KDS folder:

C:\Freescale\KDS_3.0.0\doc\KDS_Porting_Guide.pdf

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,700 Views
jacquesnapoleon
Contributor I

Hi Fiona,

Thanks to confirm what was mentioned earlier by other people above...

Anyway, as a suggestion this could help to enhance getting started manual by including starting from scratch procedures with KDS and available examples for this IDE if any...

Thanks and regards,

Jacques.

0 Kudos
1,700 Views
jacquesnapoleon
Contributor I

Hello Alice,

Thanks for you reply.

Actually KE02-SC examples do not support KDS but these are the only available examples that can be found at KDS download web page...

Thanks again.

Jacques.

0 Kudos
1,700 Views
BlackNight
NXP Employee
NXP Employee

Hi Jacques,

There is a CodeWarrior project converter in KDS:

pastedImage_0.png

It might not be able to convert anything, but should help you getting the project to KDS.

I hope this helps,

Erich

0 Kudos
1,700 Views
jacquesnapoleon
Contributor I

Hi Erich,

Thanks for your support.

I will try to convert my project file following your instructions and will let you know.

Jacques.

0 Kudos
1,701 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jacques,

Does your KE02-SC example support KDS ?

In my hand ,it only support CW ,IAR and KEIL .

pastedImage_0.png

Hope it helps

Alice

0 Kudos