AnsweredAssumed Answered

MQX K53 custom board configuration

Question asked by Alberto Peña on Aug 26, 2015
Latest reply on Aug 28, 2015 by soledad

Hi

I'm using a MK53DN512CMD10 microcontroller on a custom board with a external cristal 8MHz and MQX.

I made a bsp clon with the BSP cloning wizard and tried to configure the clock reference using processor expert.

When i try to run code it got stuck in the next line at the dispatch.S file:

 

ASM_LABEL(no_one_to_run)

                /* woohoo, idle task must be enabled, this point cannot be reachable, you have serious problem */

               b .

I have a couple of questions:

¿Can MQX on a K53DN512 work with a external cristal ?

¿How do i configure MQX clock?

 

I´ll be thankful for your answer

Regards

Alberto Peña

Outcomes