AnsweredAssumed Answered

USB_Class_CDC_Init()

Question asked by Audi McAvoy on Aug 26, 2015
Latest reply on Sep 16, 2015 by Kerry Zhou

Okay, I'll bite.

 

What do I need to include to use USB_Class_CDC_Init()?

 

I created a new, bare metal, FRDM-K64F project.  I used KSDK 1.2 and PEx.  I added an fsl_usb_descriptors component, edited it, and Generated Processor Expert Files.

 

Now I want to call USB_Class_CDC_Init().  The only header file I can find that references it is usb_class_cdc.h, but it declares the function as extern.

extern usb_status USB_Class_CDC_Init(...);

 

I can see that usb_cdc.c actually defines the function; but, usb_cdc.h does not expose it.

 

Since I've already built the demo project, I have a usb_cdc.o available.  How do I tell my project to use it?

- Audi

Outcomes