AnsweredAssumed Answered

Basic T1040RDB PCIe connection

Question asked by Felix Osuna Cotto on Aug 18, 2015
Latest reply on Aug 25, 2015 by Yiping Wang

Hello,

 

I'm very new with the T1040RDB board and PCIe. Basically,what I'm trying to do is transfer memory from a PC to my T1040RDB dev board via a PCIe connection. I have currently have default settings on my dev board. First, I want to recognize the dev board on my PC. I have a PCIe to PCIe cable that doesn't transfer power (because I don't have a need for power). The plan is to connect one end into the PC motherboard PCIe slot and the other into the dev board PCIe slot. I was just wondering if there would be any hardware/electrical issues (e.g. the the ref clk)? Do I need to configure the RCW on the dev board to be an end-point first? Any help getting started would be greatly appreciated. Thanks.

 

 

Felix

Outcomes