Hy all,
I'm in a big trouble with KDS, and i don't know, how to solve it. The problem is that I wrote a program that communicate with multiple devices on MODBUS, and I can't monitoring the processes with the breakpoints. If I build my own program first, it works without any failure. After that, when I open an other project and than build and run it, it won't be able to work, and if I turn back to my first project, it won't be, too. My program doesn't receive any data from the devices, so if I put a breakpoint to the OnReceiveBlock function, nothing happens. In practice, I can measure the output pin with a scope, and I have to push the reset button a lot to make my project OK.
Maybe this message helps, but I don't know, what does it mean:
No source available for "(gdb[2].proc[42000].threadGroup[i1],gdb[2].proc[42000].OSthread[1]).thread[1].frame[0]"
Sometimes, after a build it says: "No source for 0x"address""
I really don't know, if my settings are good, but I have an old project, that uses the similar peripherals, and it's working with no problem.
I'm using a P&E Multilink Universal external debugger.(without that, the result is the same).
Can you help me to figur out, what am I doing wrong, ot what's the matter?
Kinetis version number: 2.0.0
Operating System: Ubuntu Linux
KDS v2.0.0 is pretty old. Can you use v3.0.0 (no need to uninstall v2.0.0, just install v3.0.0 into a different folder).
Because v3.0.0 comes with a new gdb, so most likely your problem will go away.
I hope this helps,
Erich
Hy all,
I have developed a Processor Expert project with CW 10.6 on MK20DX256VLL10 microprocessor but with that program I have encountered problems with Flashing on my board. So I have transfered my project on KDS v3.0.0 and after many corrections with import I had same Adams' problem .
I used GDB PEMicro Interface Debugging as Debugger Configuration.
Can you help me to figure out, what am I doing wrong or some way to come over this GDB bug?
Operating System: Windows 7 Home Premium