Hi
I followed the tutorial to start the demo program on my FRDM-k64
with KDS on MAC Yosemite
I installed the SDK and installed software in the IDE
then I build the first project as shown, when I go to Debug Configurations
I can;'t see openSDA at all
on PEMicro section I can see OpenSDA Embedded Debug - USB port
but in the port section below nothing is shown
when I try to run->flash from file
I can ONLY see GDG SEGGER and nothing else (at least in debug I can see more)
and I can't flash my device
The device works only with the online ARM compiler
Please help because I'm desperately trying to find what is missing.
I followed the instructions twice but something is different for me
Thanks
Simone !
Hello Simone,
Please, load the firmware for your FRDM-K64F.
You can refer to: Segger J-Link Firmware for OpenSDAv2 | MCU on Eclipse
For getting to bootloader mode please follow these steps:
Unplug the USB cable (if attached).
2.Press and hold the Reset button.
3.Plug in a USB cable from a USB Host to the OpenSDA USB port.
4.Release the RESET/Bootloader button.
5.A removable drive will be visible in the host file system with a volume label of BOOTLOADER.
After that you must see in J-Link Debugger in KDS correctly filled port
and see it in Device Manager
Please, let us know, if it helps you.
Best Regards,
Iva
HI Simone,
Unlike the Windows and Linux versions of KDS, which support SEGGER, PEMicro, and OpenOCD debug configurations. The Mac version of KDS only supports SEGGER debug configurations (New Kinetis Design Studio V3.0.0 available).
If you're trying to use the SEGGER OpenSDA application (SEGGER - The Embedded Experts - OpenSDA / OpenSDA V2), then simply create a normal SEGGER debug configuration. There is no need to tell a SEGGER debug configurations that you are using OpenSDA; the board will appear to your computer as a SEGGER J-Link.
Hope that helps,
Hello Simone,
Please select the SEGGER J-Link to download :
Hope it helps
Alice