AnsweredAssumed Answered

K53 BSP stuck in line ASM_LABEL(no_one_to_run) dispatch.S file

Question asked by Jose Flores on Aug 13, 2015
Latest reply on Sep 1, 2015 by soledad

Good morning,

 

I made a custon PCB with the MK53DN512CMD10 microcontroller. I´m trying to run a simple code and it got stuck in the next line at the dispatch.S file:

 

ASM_LABEL(no_one_to_run)

                /* woohoo, idle task must be enabled, this point cannot be reachable, you have serious problem */

               b .

 

I´m using an 8 MHz external crystal on PTA18 and PTA19, I already configured the ProcessorExpert.pe (System oscillator -  Clock source = External and Clock frequency = 8MHz) and I generate de code on Generate Processor Expert Code option. If it helps, appears the next warning:

 

DescriptionResourcePathLocationType
Warning: The PLL/FLL clock value is 0 - the clock is disabled. (Clock frequency [MHz])bsp_twrk53n512Cpu/Clock frequency [MHz]Processor Expert Problem

 

And I can´t chance the option to able.

 

What should I do?

 

Best regards.

Outcomes