I have bought a new SABRE board for smart devices base on the I.MX6 series,but when I luanch the board,it post the message below on the screen:
egulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:01 UTC (1)
Freeing init memory: 244K
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
android_usb: already disabled
android_usb: already disabled
mtp_bind_config
root@android:/ # input: eCompass as /devices/virtual/input/input7
mxc_hdmi mxc_hdmi: same edid
mxc_hdmi mxc_hdmi: same edid
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: v4l2 capture: slave not found!
ERROR: HDMI is not ready!
asoc: can't open platform imx-hdmi-soc-audio.0
mxc_hdmi mxc_hdmi: same edid
mxc_hdmi mxc_hdmi: same edid
mxc_hdmi mxc_hdmi: same edid
mxc_hdmi mxc_hdmi: same edid
what's wrong with the board ,please help me out.
Solved! Go to Solution.
Hello !
Please check / change HDMI cable.
If You are using HDMI/DVI converter :
It is required to add new 'allow_noncea=1' environment variable in the U-Boot
configuration and the arguments to set resolution to the kernel command line ;
as an example
'video=mxcfb0:dev=hdmi,1280x1024M@60,if=RGB24'.
Also, the following may be helpful :
"HDMI Error on I.MX6Q SDB"
https://community.freescale.com/thread/302840
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello !
Please check / change HDMI cable.
If You are using HDMI/DVI converter :
It is required to add new 'allow_noncea=1' environment variable in the U-Boot
configuration and the arguments to set resolution to the kernel command line ;
as an example
'video=mxcfb0:dev=hdmi,1280x1024M@60,if=RGB24'.
Also, the following may be helpful :
"HDMI Error on I.MX6Q SDB"
https://community.freescale.com/thread/302840
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thank you to reply,I have solved the problem under your advice.thank you very much!