Hi,
I have a problem loading the program to the MCU, because when try to load the compiled code into the flash memory, appears the error.:
ELF Loader: Error while writing to 4000 - 4200
Information no memory at this address.
The behavior is abnormal because previously I have been doing the same procedure, but with the result of a successful load on the MCU firmware.
Maybe a sector of the flash is corrupt?
What does the error?
Why could Happen error?
Thank you very much for your help,
MC9S12E128CPV
CoderWarrior 5.9
P&E Micro USB Multilink Interface
Solved! Go to Solution.
Hi Rene,
Difficult to know exactly what is the problem.
I think the better solution should be to create a new project with your hardware configuration and to add the source files you're using.
Now if you're using Processor Expert, you can create a project including Processor Expert and chang the .pe file too in the new project.
But if the problem is linked to wrong/corrupted Processor Expert configuration you will need to re-create the PEx configuration.
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Rene,
I think you should use CW for HCs12 V5.1 development tool.
It seems you were able to load the application on board and not anymore ...
Do you change something in your project ?
Do you use Processor Expert ?
do you tried with an demo example created with the wizard ?
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pascal,
Thanks for your help. I tried with another project that i loaded before and works!, so i suppose that the project was corrupted. By another hand, i'm using just a folder that contains the project but it wasn't have the .xml file (from import project) and followings warnings was displayed:
The following access path in target "P&E ICD" of project "proyecto" cannot be found:
{Project}cmd
{Compiler}\bin\Pluggins\support\ProcessorExpert\PESL\HCS12
{Compiler}\bin\Pluggins\support\ProcessorExpert
The following access path in target "Simulator of project "proyecto" cannot be found:
{Project}cmd
And i think that a lack of path for Processor Expert could be corrupting the project, when i activate the PE in the project, what do you think? do you have any recomendation ?
Thanks
Hi Rene,
Difficult to know exactly what is the problem.
I think the better solution should be to create a new project with your hardware configuration and to add the source files you're using.
Now if you're using Processor Expert, you can create a project including Processor Expert and chang the .pe file too in the new project.
But if the problem is linked to wrong/corrupted Processor Expert configuration you will need to re-create the PEx configuration.
Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------