AnsweredAssumed Answered

ADC cross reference

Question asked by Ken Armitage on Aug 12, 2015
Latest reply on Aug 12, 2015 by soledad

Hi...

 

I hope I'm posting this to the right place, as my question really spans MQX and the bsp files related to the TWRK60 boards....

 

Is there a simple list or table somewhere that cross references the pin-out of a specific device to the pin of the ADC.

 

For example on the TWR-K60DM board, the potentiometer is connected to pin K2 which on the schematic is described as ADC1_DM1.

 

 

In the bsp.h file the input is defined as;

 

 

#define BSP_ADC_CH_POT                  (ADC1_SOURCE_AD20)...?

 

How do you relate the two...?

 

Thanks

 

Ken

 

 

 

Outcomes