AnsweredAssumed Answered

how to load program to internal flash in KDS using pe micro

Question asked by Lijo Francis on Aug 11, 2015
Latest reply on Aug 11, 2015 by ZhangJennie

Dear sir,

i am using K60 tower board ..with PE Micro programmer.we load the code using Debug mode........That code is loaded and its running and its working very much.....

when i power off then i power on , the code i loaded using debug mode not running..........

why the code not running is that code loaded into ram....how can i load the code into flash....if that code load into flash why that code not running after restart...

in kds there is no option to load the code into flash...but i have seen in code warrior there is option for ram or flash...................................

 

We tried kds 2.0 file to flash but that not working

please tell me its very urgent

Outcomes