AnsweredAssumed Answered

Quick Read Streaming for K64F-AGM01

Question asked by Gert Jan Hoeve on Aug 11, 2015

Hi,

 

I have a sensor board STBC-AGM01 on a K64F development board. I installed the Freedom Sensor Tooblbox, together with a couple of example streaming files to send to the board using the Kinetis Interface Tool v2, and read out the raw sensor values. They work fine, except for the fact that the stream stops after about five minutes. Is that an intended feature of the demo program? Because I would like to sample much longer than that. (I already excluded Windows Power Management closing the USB port as a possible cause.)

 

The command stream I used: (Subscription 1 Quick Read Streaming Commands.txt)

 

0x01 0x01 0x06 0x00 0x00  // Reset MBOX

0x01 0x02 0x06 0x00 0x00  // Reset APP

0x01 0x01 0x02 0x2C 0x0C 0x02 0x0A 0x02 0x0B 0x02 0x0C 0x02 0x0D 0x02 0x0E 0x02 0x0F  // TS + Subscription #1

0x01 0x01 0x02 0x18 0x14 0x02 0x00 0x02 0x01 0x02 0x02 0x02 0x03 0x02 0x04 0x02 0x05 0x02 0x06 0x02 0x07 0x02 0x08 0x02 0x09  // TS + Subscription #2

0x01 0x01 0x02 0x38 0x01 0x04  // Enable CI Streaming

0x01 0x02 0x02 0x00 0x01 0x52  // Start APP Streaming

Outcomes