AnsweredAssumed Answered

Gplay options via command line

Question asked by Manjunath Joshi on Aug 10, 2015
Latest reply on Aug 11, 2015 by Yuri Muhin

Hello all,

 

I am keen to know if gplay has command line options to set the volume or to mute.

 

When i do gplay --help on command prompt, only

 

gplay file_list

 

is shown.

 

But when i play using gplay sample.mp3,

 

i get options to pause,play,stop,mute etc.

 

My intention is to control the options via command line at the command gplay execution itself not while it is playing.

 

Regards,

Manju

Outcomes