Hi All,
Platform : imx6sl
Os : Android kitkat 4.4.3
I made my module to run as wifi and bluetooth individually, but not I want to make it coexist. For that do I need to enable anything in the Android BSP????
Please suggest me how to proceed from here???
Thanks and Regards,
Mutyalarao.
Hi mutyalarao
bluetooth and wifi stacks need to speak to each other to know when
is an appropriate time to prefer wifi traffic or bluetooth traffic and AR6103
has special signals called Bluetooth Coexistence Interface, however these signals
are not routed on connector on Sabre board.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------