The reason I ask is that I ended up using P&E's driver install which puts a Jungo Windriver driver in the system. The problem is that I already had a Jungo Windriver for my IAR Atmel JTAGICE3 which gets overwritten by the P&E one. So I can't use my IAR Atmel tools and the KDS Multilink Universal without uninstalling the corresponding Windriver that each one needs. Any way for more than one Windriver to exist at the same time? If KDS supports the Universal directly without installing the P&E driver then that would be great so I can keep the IAR one.
hi Phil.
by default, KDS can support P&E Multilink Universal FX without driver. on my computer i can use it without driver.
P&E also provides separate driver for it, we can download USB Multilink Universal Resource CD from this url:
please make sure the firmware in Multilink Universal FX is for the specific chip you are using.
can this help you?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------