AnsweredAssumed Answered

Even if SuperRootKey differ, in Open-Mode, we can see No HAB Event.

Question asked by George Fukutomi on Aug 9, 2015
Latest reply on Aug 21, 2015 by George Fukutomi

Dear All,

 

We certified Code using cst-2.3.1.

It is working correctly in Open-Mode and Closed-Mode.

However, we have one question.

 

The device which burned different SuperRootKey is not boot in Closed-Mode-Configuration.

However, Also on the device which burned different SuperRootKey in Open-Mode-Configuration, we can see No HAB Event.

 

I can understand boot also on device which burned different SuperRootKey in Open-Mode-Configuration, and I think that it has some HAB Event.

However, it does not have HAB Event.

 

Is this the correct behavior?

 

Best Regards,

George

Outcomes