Cache flush/invalidate in MPC5554/e200z6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cache flush/invalidate in MPC5554/e200z6

Jump to solution
1,805 Views
ricardofranca
Contributor II

Hello,

 

I am doing some experiments with the e200z6 unified cache - specifically, I'm analyzing the effects of flushing and invalidating the entire cache in some application. Currently, I'm invalidating and flushing each cache line individually:

 

/* GreenHills compiler asm syntax */

 

__asmleaf void flush_inv_cache_line(unsigned int flushed_way, unsigned int flushed_set) {

%reg flushed_way %reg flushed_set

mfspr r3, l1finv0

insrwi r3, flushed_way, 5, 3

insrwi r3, flushed_set, 7, 20

li r4, 2

rlwimi r3, r4, 0, 30, 31

msync

mtspr l1finv0, r3

    }

 

void flush_inv_cache(void) {

    unsigned int i;

    unsigned int j;

    for (i = 0u; i < 8u; i++)

    {

        for (j = 0u; j < 128u; j++)

        {

            flush_inv_cache_line(i, j);

        }

    }

}

 

It seems the code is working correctly, but I wonder if there are more efficient ways of doing this. Is there any way to flush and invalidate the entire cache without these loops?

 

Best regards,

 

Ricardo

Labels (1)
0 Kudos
1 Solution
1,223 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Ricardo,

that's a good point. When the cache is invalidated using CINV bit, data are not flushed. This operation is not supported on the device. So, it could cause cache coherency issues. If you use copyback mode, the only way to flush the cache is to use L1FINV0 register and flush each cache line individually.

Regards,

Lukas

View solution in original post

3 Replies
1,223 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

this can be found in core reference manual for e200z6:

pastedImage_0.png

Regards,

Lukas

0 Kudos
1,223 Views
ricardofranca
Contributor II

Hi Lukas,

Thanks for your answer. When reading the e200z6 documentation, I wondered if doing an invalidation in the way you show could create cache coherency issues if I use the cache in copyback mode. How does data/instruction copyback work when I set L1CSR0[CINV]?

Best regards,

Ricardo

0 Kudos
1,224 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Ricardo,

that's a good point. When the cache is invalidated using CINV bit, data are not flushed. This operation is not supported on the device. So, it could cause cache coherency issues. If you use copyback mode, the only way to flush the cache is to use L1FINV0 register and flush each cache line individually.

Regards,

Lukas